Skip to main content
Nickname2530_O
Visitor II
May 26, 2014
Question

VL6180X : What are the basic features ?

Posted on May 26, 2014 at 09:10

What are the basic features of VL6180X ?

#vl6180x #features
This topic has been closed for replies.

2 replies

Colin RAMRATTAN
Visitor II
May 26, 2014
Posted on May 26, 2014 at 20:20

The VL6180X allows any user to measure the distance of any object within a 0 to 100mm range from the sensor regardless of the reflectivity of the material. Along with the distance measured, the VL6180X gathers information on the amount signal and noise entering into the sensor which allows the VL6180X to measure the distances of these objects in any lighting environment.

The VL6180X also allows a user to measure the amount of ambient light with the built in ambient light sensor. With a simple math equation the equivalent lux value can be obtained from the measurement stored in the VL6180X.

maricic
Visitor II
February 6, 2015
Posted on February 06, 2015 at 20:33

What is the sampling rate range for the ambient light sensor?