Skip to main content
tlock
Visitor II
March 26, 2015
Question

VL6180X supply voltage

Posted on March 26, 2015 at 15:40

The VL6180X's typical supply voltage is listed as 2.8V.  Is there any problem with operating it at 3.3V which is less than the 3.6V absolute maximum?

This topic has been closed for replies.

1 reply

Nickname681_O
Visitor II
March 26, 2015
Posted on March 26, 2015 at 16:33

Thomas,

The maximum functional operational voltage is 3.0V.  Running the device at higher voltage is not suggested.  It will not operate according to the specified operation parameters.    The absolute maximum value for the supply voltage indicates the limit at which supplying a voltage above that limit (3.6V)  may cause damage to the part.

Ken W @ST