A while back we had a lot of questions like this. So instead of reading complex manual and trying to figure it all out, we wrote an API that does it all for you.
That API can be found at:
STSW-IMG003
Even if you don't use the API, there is a function in there that will set the max convergence time for you.
And look it over for other routines you might need.
And if you are so inclined - just use the API in your project. All the functions have been validated.
The following is what that API does. Compare it to yours.
good luck
static int VL6180x_RangeSetEarlyConvergenceEestimateThreshold(VL6180xDev_t dev)
{
int status;
const uint32_t cMicroSecPerMilliSec = 1000;
const uint32_t cEceSampleTime_us = 500;
uint32_t ece_factor_m = VL6180xDevDataGet(dev, EceFactorM);
uint32_t ece_factor_d = VL6180xDevDataGet(dev, EceFactorD);
uint32_t convergTime_us;
uint32_t fineThresh;
uint32_t eceThresh;
uint8_t u8;
uint32_t maxConv_ms;
int32_t AveTime;
LOG_FUNCTION_START("");
do {
status = VL6180x_RdByte(dev, SYSRANGE_MAX_CONVERGENCE_TIME, &u8);
if (status) {
VL6180x_ErrLog("SYSRANGE_MAX_CONVERGENCE_TIME rd fail");
break;
}
maxConv_ms = u8;
AveTime = _GetAveTotalTime(dev);
if (AveTime < 0) {
status = -1;
break;
}
convergTime_us = maxConv_ms * cMicroSecPerMilliSec - AveTime;
status = VL6180x_RdDWord(dev, 0xB8, &fineThresh);
if (status) {
VL6180x_ErrLog("reg 0xB8 rd fail");
break;
}
fineThresh *= 256;
eceThresh = ece_factor_m * cEceSampleTime_us * fineThresh / (convergTime_us * ece_factor_d);
status = VL6180x_WrWord(dev, SYSRANGE_EARLY_CONVERGENCE_ESTIMATE, (uint16_t)eceThresh);
} while (0);
LOG_FUNCTION_END(status);
return status;
}
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.