Skip to main content
TBoul.1
Visitor II
August 27, 2020
Question

VL6180x distance issue

  • August 27, 2020
  • 1 reply
  • 612 views

Hi,

We are using VL6180X to measure the cyclic movement of a part (a flat, white plastic sheet). The amplitude of this cyclic movement is about 20mm. The distance sensors work fine but we had two recent instances where the distance sensors returned a correct amplitude and then suddenly returned a reduced amplitude of 5mm only. After resetting the sensor, measurements came back to normal.

Have you ever observed such behavior? What could explain that?

Thank you

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
October 6, 2020

Yes unfortunately I have. The issue is that every now and again you are querying the sensor at just the wrong moment and it interupts a critical bit of code. The result is basically random number.

Download the latest API.

In it you will see a correction:

  VL6180_WrByte(dev, 0x00e3, 0x01); //was 0x00

 VL6180_WrByte(dev, 0x00e4, 0x03); //was 0x04

You can just update those two lines in your initialization and it will fix the issue.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.