Skip to main content
Ben1
Associate III
November 20, 2020
Question

VL53LX Range sensor API size optimization

Hi everyone,

I try to implement range measurement using the VL53L3CX sensor with the VL53L3CX_API_1.1.4. I can get distance measurement and talk with the sensor properly using the basic patent :

Status = VL53LX_WaitDeviceBooted(Dev);
Status = VL53LX_DataInit(Dev);
Status = VL53LX_StartMeasurement(Dev);
 
for(;;)
{
Status = VL53LX_WaitMeasurementDataReady(Dev);
Status = VL53LX_GetMultiRangingData(Dev, pMultiRangingData);
printf("d= %5dmm",pMultiRangingData->RangeData[j].RangeMilliMeter);
}

The issue is : I have FLASH memory overflowed with .data and user data when it comes to add my applicaction! (by 17kB!!) :fearful_face:

I don't need to detect more than 1 object, and I don't need precision nor any calculation feature but the ones strictly needed to have distance. Is there any functions or c files I could get rid of?

I tried to mess around with the API but there are quite a lot of things! I took a look at the VL53LX_DataInit() for instance. It calls VL53LX_data_init() :

VL53LX_Error VL53LX_data_init(
	VL53LX_DEV Dev,
	uint8_t read_p2p_data)
{
 
 
	VL53LX_Error status = VL53LX_ERROR_NONE;
	VL53LX_LLDriverData_t *pdev =
			VL53LXDevStructGetLLDriverHandle(Dev);
	VL53LX_LLDriverResults_t *pres =
			VL53LXDevStructGetLLResultsHandle(Dev);
 
 
 
	VL53LX_zone_objects_t *pobjects;
 
	uint8_t i = 0;
 
	LOG_FUNCTION_START("");
 
	VL53LX_init_ll_driver_state(
			Dev,
			VL53LX_DEVICESTATE_UNKNOWN);
 
	pres->range_results.max_results = VL53LX_MAX_RANGE_RESULTS;
	pres->range_results.active_results = 0;
	pres->zone_results.max_zones = VL53LX_MAX_USER_ZONES;
	pres->zone_results.active_zones = 0;
 
	for (i = 0; i < VL53LX_MAX_USER_ZONES; i++) {
		pobjects = &(pres->zone_results.VL53LX_p_003[i]);
		pobjects->xmonitor.VL53LX_p_016 = 0;
		pobjects->xmonitor.VL53LX_p_017 = 0;
		pobjects->xmonitor.VL53LX_p_011 = 0;
		pobjects->xmonitor.range_status =
				VL53LX_DEVICEERROR_NOUPDATE;
	}
 
 
 
	pres->zone_hists.max_zones = VL53LX_MAX_USER_ZONES;
	pres->zone_hists.active_zones = 0;
 
 
 
	pres->zone_cal.max_zones = VL53LX_MAX_USER_ZONES;
	pres->zone_cal.active_zones = 0;
	for (i = 0; i < VL53LX_MAX_USER_ZONES; i++) {
		pres->zone_cal.VL53LX_p_003[i].no_of_samples = 0;
		pres->zone_cal.VL53LX_p_003[i].effective_spads = 0;
		pres->zone_cal.VL53LX_p_003[i].peak_rate_mcps = 0;
		pres->zone_cal.VL53LX_p_003[i].median_range_mm = 0;
		pres->zone_cal.VL53LX_p_003[i].range_mm_offset = 0;
	}
 
	pdev->wait_method = VL53LX_WAIT_METHOD_BLOCKING;
	pdev->preset_mode = VL53LX_DEVICEPRESETMODE_STANDARD_RANGING;
	pdev->zone_preset = VL53LX_DEVICEZONEPRESET_NONE;
	pdev->measurement_mode = VL53LX_DEVICEMEASUREMENTMODE_STOP;
 
	pdev->offset_calibration_mode =
		VL53LX_OFFSETCALIBRATIONMODE__MM1_MM2__STANDARD;
	pdev->offset_correction_mode =
		VL53LX_OFFSETCORRECTIONMODE__MM1_MM2_OFFSETS;
	pdev->dmax_mode =
		VL53LX_DEVICEDMAXMODE__FMT_CAL_DATA;
 
	pdev->phasecal_config_timeout_us = 1000;
	pdev->mm_config_timeout_us = 2000;
	pdev->range_config_timeout_us = 13000;
	pdev->inter_measurement_period_ms = 100;
	pdev->dss_config__target_total_rate_mcps = 0x0A00;
	pdev->debug_mode = 0x00;
 
	pdev->offset_results.max_results = VL53LX_MAX_OFFSET_RANGE_RESULTS;
	pdev->offset_results.active_results = 0;
 
 
 
	pdev->gain_cal.standard_ranging_gain_factor =
			VL53LX_TUNINGPARM_LITE_RANGING_GAIN_FACTOR_DEFAULT;
	pdev->gain_cal.histogram_ranging_gain_factor =
			VL53LX_TUNINGPARM_HIST_GAIN_FACTOR_DEFAULT;
 
 
	VL53LX_init_version(Dev);
 
 
	memset(pdev->multi_bins_rec, 0, sizeof(pdev->multi_bins_rec));
	pdev->bin_rec_pos = 0;
	pdev->pos_before_next_recom = 0;
 
 
 
	if (read_p2p_data > 0 && status == VL53LX_ERROR_NONE)
		status = VL53LX_read_p2p_data(Dev);
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_refspadchar_config_struct(
			&(pdev->refspadchar));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_ssc_config_struct(
			&(pdev->ssc_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_xtalk_config_struct(
			&(pdev->customer),
			&(pdev->xtalk_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_xtalk_extract_config_struct(
			&(pdev->xtalk_extract_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_offset_cal_config_struct(
		 &(pdev->offsetcal_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_zone_cal_config_struct(
			&(pdev->zonecal_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_hist_post_process_config_struct(
			pdev->xtalk_cfg.global_crosstalk_compensation_enable,
			&(pdev->histpostprocess));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_hist_gen3_dmax_config_struct(
			&(pdev->dmax_cfg));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_init_tuning_parm_storage_struct(
			&(pdev->tuning_parms));
 
	if (status == VL53LX_ERROR_NONE)
		status = VL53LX_set_preset_mode(
			Dev,
			pdev->preset_mode,
			pdev->dss_config__target_total_rate_mcps,
			pdev->phasecal_config_timeout_us,
			pdev->mm_config_timeout_us,
			pdev->range_config_timeout_us,
			pdev->inter_measurement_period_ms);
 
	VL53LX_init_histogram_bin_data_struct(
			0,
			VL53LX_HISTOGRAM_BUFFER_SIZE,
			&(pdev->hist_data));
 
	VL53LX_init_histogram_bin_data_struct(
			0,
			VL53LX_HISTOGRAM_BUFFER_SIZE,
			&(pdev->hist_xtalk));
 
 
	VL53LX_init_xtalk_bin_data_struct(
			0,
			VL53LX_XTALK_HISTO_BINS,
			&(pdev->xtalk_shapes.xtalk_shape));
 
 
 
	VL53LX_xtalk_cal_data_init(
			Dev
			);
 
 
 
	VL53LX_dynamic_xtalk_correction_data_init(
			Dev
			);
 
 
 
	VL53LX_low_power_auto_data_init(
			Dev
			);
 
#ifdef VL53LX_LOG_ENABLE
 
 
 
	VL53LX_print_static_nvm_managed(
		&(pdev->stat_nvm),
		"data_init():pdev->lldata.stat_nvm.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_customer_nvm_managed(
		&(pdev->customer),
		"data_init():pdev->lldata.customer.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_nvm_copy_data(
		&(pdev->nvm_copy_data),
		"data_init():pdev->lldata.nvm_copy_data.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_dmax_calibration_data(
		&(pdev->fmt_dmax_cal),
		"data_init():pdev->lldata.fmt_dmax_cal.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_dmax_calibration_data(
		&(pdev->cust_dmax_cal),
		"data_init():pdev->lldata.cust_dmax_cal.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_additional_offset_cal_data(
		&(pdev->add_off_cal_data),
		"data_init():pdev->lldata.add_off_cal_data.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_user_zone(
		&(pdev->mm_roi),
		"data_init():pdev->lldata.mm_roi.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_optical_centre(
		&(pdev->optical_centre),
		"data_init():pdev->lldata.optical_centre.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
	VL53LX_print_cal_peak_rate_map(
		&(pdev->cal_peak_rate_map),
		"data_init():pdev->lldata.cal_peak_rate_map.",
		VL53LX_TRACE_MODULE_DATA_INIT);
 
#endif
 
	LOG_FUNCTION_END(status);
 
	return status;
}

Do we need to set ALL the data in this function? Don't the VL53LCX have any default parameters which could avoid to call all these sub-functions? This is juste an example.

In the case I have to bypass some functions, I am not afraid to get through the entire API to delete/comment all occurences of these functions.

Any suggestion is appreciated, thank you in advance for your help! :beaming_face_with_smiling_eyes:

    This topic has been closed for replies.

    2 replies

    jgnoss
    Associate III
    November 25, 2020

    there is some build in functionality

    for logging and error decoding that's normally only used for debug and test.

    I don't know if you can get rid of that by some compiler flags or defines

    have a look at

    api/src/vl53l0x_api_strings.c

    api/platform/vl53l0x_platform_log.c

    and it's header files

    ju

    SLin.11
    Associate II
    January 27, 2021

    I wish vl53l3cx can come out a reduced size API like VL53L1X did -- VL53L1X ULD API (Ultra Lite Driver API).

    That will be great.

    sam