Skip to main content
leo su
Associate II
May 23, 2018
Question

VL53L1 sensors activate without expansion board but by using SHUT pin on/off

Posted on May 23, 2018 at 14:05

We use VL53L1 connected to our MCU board without xVL53L1 expansion board as DevId = 0/1/2...

By using MCU controlling the IO to off/on the XSHUT pin of sensor but during init. process,

it fails at 

VL53L1_WaitDeviceBooted() with error message, 

VL53L1_ERROR_CONTROL_

INTERFACE

flow is as below:

1. XSHUT with all 3 sensor to low for device-disable.

2. each enable by XSHUT to high with standard init process as example code suggests

-> it fails at this stage, (I2C seems not working..,,. is it related with 

==

/* 2V8 power mode selection codex 447463 */

#ifdef USE_I2C_2V8

Status = VL53L1_RdByte(Dev, VL53L1_PAD_I2C_HV__EXTSUP_CONFIG, &i);

if (Status == VL53L1_ERROR_NONE) {

i = (i & 0xfe) | 0x01;

Status = VL53L1_WrByte(Dev, VL53L1_PAD_I2C_HV__EXTSUP_CONFIG,

i);

}

#endif

==

but it is called at fun VL53L1_DataInit() after 

VL53L1_WaitDeviceBooted() and this will cause

I2C action failure during 

VL53L1_WaitDeviceBooted(), any help?

This topic has been closed for replies.

2 replies

leo su
leo suAuthor
Associate II
May 28, 2018
Posted on May 28, 2018 at 05:50

By the way,

we try using only 1 sensor without expander board but using GPIO1 to shut off/turn on the sensor

and however it doesn' t work either. We find I2C bus is not workable..... don't know any other feasibility consideration that we missed???

leo su
leo suAuthor
Associate II
May 28, 2018
Posted on May 28, 2018 at 08:02

Our supply voltage is v3.3, not v2.8, is that the problem of it?