Skip to main content
Mariia_Volkova_22
Visitor II
March 7, 2019
Question

VL53L0X. What function or algorithm should I use to read the values from the sensor VL53L0X with protective glass? What parameter should I change with this?

Hello everyone!

I use an obstacle detection sensor VL53L0X. I had a problem using protective glass. I use VL53L0X_API_v1.0.2.4823_externalx. When I put the glass in front of the sensor with the correct clearances, I get a strange distance. When there is no obstacle in front of the sensor, it shows about 20-30 mm, and when I put an obstacle, the sensor shows the correct distance to the obstacle, but in a small range. Everything corresponds to the cross-talk picture. Please tell me which parameter I need to change in the code. What parameter is responsible for this? Is there an algorithm that takes into account the use of protective glass?

Thank you.

    This topic has been closed for replies.