Skip to main content
TGund
Associate
February 12, 2020
Question

Vl53L0X Offset Calibration

Hello,

I am currently trying to implement offset calibration to VL53L0X sensor. I placed sensor in front of white paper with 100mm distance as datasheet suggest. When I get sensor measurement before offset calibration, I get 135mm which is fine because i placed glass in front of the sensor. However, when I calibrate sensor, I get 0mm as a result from same distance. So, I move sensor to 200mm, I am getting 100mm for measurement. I think of offset calibration as it will add or subtract offset value from the measurement value not set 0mm when the offset calibration has made. I am using VL53L0X_perform_offset_calibration function from api. I followed UM2039 documentation as referance. So, what could be the possibble reason for that or is it the way offset calibration work?

Regards,

Taha

This topic has been closed for replies.

1 reply

FPayn.1
Associate III
July 20, 2020

Taha,

I'm just a VL53L0X novice like yourself, so I probably know less than you do about offset calibration. However, looking at the documentation for VL53L0X_PerformOffsetCalibration(), I see that one parameter is

 * @param  CalDistanceMilliMeter   Calibration distance value used for the

 * offset compensation.

Is it possible that you didn't provide this value? Also, it appears that the last parameter for this call is a pointer that will be updated to point to a location containing a 32-bit integer that is the new offset value - in micrometers; could you check to see what that new value is after you do the calibration?

Just my $0.02 ;)

Frank