Skip to main content
Julien NGUYEN
ST Employee
June 13, 2019
Question

VL53L0X MBED libraries

  • June 13, 2019
  • 3 replies
  • 1698 views

Where to find the VL53L0X MBED libraries ?

    This topic has been closed for replies.

    3 replies

    Julien NGUYEN
    ST Employee
    June 13, 2019

    ​You can find the VL53L0X MBED here below

    https://os.mbed.com/teams/ST/code/VL53L0X/

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    Joel von Rotz
    Associate
    June 13, 2019

    Thanks for the link, but is there a way to make it compatible with the LPC1768?

    The library uses other libraries, like the X_NUCLEO_COMMON, ST_INTERFACES and STMPE1600. Since the LPC1768 doesn't use the STMPE1600, is it possible to send a NULL instead of a STMPE1600 object? Wait, I didn't realize there was a VL53L0X constructor without the STMPE1600 object

    Is it possible to provide example programs with this library?

    joel.vonrotz
    Associate II
    July 22, 2019

    I guess not then, alright