Skip to main content
Itamar Eliakim
Associate II
March 21, 2017
Question

VL53L0X freeze after ~1 min of use

Posted on March 21, 2017 at 23:05

Hello,

I am trying to operate the VL53L0X through ADLINK I2C SEMA3.5R7 (com express) interface.

I initialized all the registers correctly according to - 

https://github.com/pololu/vl53l0x-arduino/blob/master/VL53L0X.cpp

 

after around ~1 min of use(continuously read the 16bit from 0x13) the device halts, i get 0 on all of the readings from the device and the only way i can get the results back are to initialize the device again.

Is there any error code register to get better understanding why the device freezes? 

Is there any chance that someone had same issues with this device?

I am using the satellite with 10K pull-up resistors on SDA/SCL.

Appreciate your help,

Itamar

#vl53l0x
This topic has been closed for replies.