Skip to main content
Associate
Apr 18, 2025 9:49 AM UTC
Question

Using the STM drivers with kernel above 6.6 i.e 6.13

Hi,
im currently working on interfacing the STM mems sensors with Beagle Vahead board, im using a kernel version of 6.13 and i tried patching the STM MEMS IIO drivers from link. Im aware that the STM has confirmed the testing of the driver with kernel 6.6.

While patching i faced few errors ie mis match in the headders and i have successfully resolved them.
im able to boot the device and able to get the device node in the /sys/bus/iio/device  when interfacing the lps22df sensor.
when any other sensors (lsm6dsox, lisduxs12,lsm6dsv32) are interfaced on the same bus, im not able to detect the device. i have the same hardware set for lps22df  also. but in that case i was able to get the raw pressure and temperature data.

I want to understand the issue why it happens so.
i have mentioned the mininal properties on the i2c bus node in DTS file. and have omitted all the optional parameters.

have a look at the STM driver booting errors

[ 1.143802] st_lsm6dsox_i2c 2-006b: supply vdd not found, using dummy regulator

[ 1.168768] st_lsm6dsox_i2c 2-006b: supply vddio not found, using dummy regulator

[ 1.177306] st_lsm6dsox_i2c 2-006b: probe with driver st_lsm6dsox_i2c failed with error -121

[ 1.186313] st_lsm6dsvx_i2c 2-006a: supply vdd not found, using dummy regulator

[ 1.194100] st_lsm6dsvx_i2c 2-006a: supply vddio not found, using dummy regulator

[ 1.202116] st_lsm6dsvx_set_page_access set page access error

[ 1.208680] st_lsm6dsvx_i2c 2-006a: probe with driver st_lsm6dsvx_i2c failed with error -121

[ 1.217828] st_lps22df_i2c 2-005c: failed to read Who-Am-I register

[ 1.224226] st_lps22df_i2c 2-005c: probe with driver st_lps22df_i2c failed with error -121

[ 1.235138] Legacy PMU implementation is available

copy of dts file where it is defined

 
&i2c2 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&i2c2_pins>;
status = "okay";
 
lis2dux12@19 {
        compatible = "st,lis2duxs12";
        reg = <0x19>;
};
 
lsm6dsox@6b {
        compatible = "st,lsm6dsox";
        reg = <0x6b>;
 
};
 
lsm6dsvx@6a {
        compatible = "st,lsm6dsv16x";
        reg = <0x6a>;
};
 
lps28dfw@5c {
        compatible = "st,lps28dfw";
        reg = <0x5c>;
};
 
 
 
};
This topic has been closed for replies.

4 replies

Federica Bossi
ST Technical Moderator
Apr 28, 2025 6:52 AM UTC

Hi @jayakrishnan_k ,

Do you see the sensors on the i2c bus using i2c-tools (like i2cdetect, i2cdump, i2cget and i2cset)?
Something like this:
# i2cdetect -y 2

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
Apr 28, 2025 7:07 AM UTC

@Federica Bossi 
yes i was able to see the sensor connected at the bus and was able to see that the sensor names mentioned in the dtb file was reflected in devices of i2c device.

but im not able to get the device in /sys/bus/iio/devices/ dir.

jayakrishnan_k_0-1745823985947.png

 

Federica Bossi
ST Technical Moderator
Apr 28, 2025 11:58 AM UTC

Hi @jayakrishnan_k ,

Okay, can you try to use a logic analyzer and send us the tracking over I2C at boot? That way we can see if there are any problems at that stage.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.