Question
Using the STEVAL-MKI122V1(LSM330DLC) by itself without the eMotions Eval Motherboard...
Posted on February 27, 2014 at 23:34
I have acquired both the STEVAL-MKI122V1(LSM330DLC) and the STEVAL-MKI109V1(eMotions Motherboard) and have been using them together for some time now. But now, I want to use the STEVAL-MKI122V1(LSM330DLC) by itself and I have figured out a way to power it and want to make sure I am powering up the LSM330DLC correctly and I am not damaging the device. I am currently applying 3V to pins 1 and 2 of the JP1 header. I am applying the Ground to pin 13 of JP2 header. Is this configuration correct?
#lsm330dlc #steval-mki122v1