Skip to main content
Christophe Thil
Visitor II
Feb 26, 2019 9:30 AM UTC
Question

Using STEVAL-MKI109V3 with Windows 10

Hi,

I struggle to use the STEVAL-MKI109V3 board with Windows 10. The VCP serial port is detected, but the OS is unable to attach the right driver (a yellow exclamation mark is shown in the Device Explorer). Other STM32 boards with USB CDC do work fine.

I tried to upgrade the firmware to version 2.40.1 (included with Unico), which seemed to be succesful.

I'd be very happy for any hints on how to operate the eval kit with Win10. Thanks.

    This topic has been closed for replies.

    4 replies

    Jacek Pieczaba
    Associate III
    Feb 26, 2019 1:10 PM UTC

    I have the same issue... If you advice us what we can do in order to make it works under Windows 10 it will be great. Thank you

    AvaTar
    Senior III
    Feb 26, 2019 1:35 PM UTC

    You could try to play with Windows options, especially compatibility settings.

    VDhan
    Associate II
    Mar 4, 2019 6:35 AM UTC

    Hello all,

    I was also facing the same issue, rather than updating the driver from device manager I resolved this issue by installing VCP_V1.5.0_Setup_W8_x64_64bits from installation folder: MEMS_Demonstration_Kit_SW_package_v8_0_WINDOWS-> Driver->STM32_vcp.

    Try this let me know if it works for you.

    Thank you

    D.Vishnu

    Jacek Pieczaba
    Associate III
    Mar 4, 2019 4:24 PM UTC

    Thank you your suggestion works very good. Have a great day​