Skip to main content
Ljian.1
Associate
June 1, 2020
Question

Use LSM6DSO to detect free-fall event can not work!

According to the official sample program, I set the register to detect free-fall event,But it can't be detected very well, even when I haven't moved anything, I have always detected the free-fall event,How can I use lsm6dso to detect free-fall event correctly?

    This topic has been closed for replies.

    4 replies

    Ljian.1
    Ljian.1Author
    Associate
    June 1, 2020

    This is the official sample program I refer to

    Eleon BORLINI
    ST Employee
    June 1, 2020

    Hi @Ljian.1​ , on which part number did you managed to detect the free-fall event, before LSM6DSO? You could try to change the detection threshold to a lower value and check if you can detect the free-fall interrupt.

     /* Set Free Fall duration to 3 and 6 samples event duration */
     lsm6dso_ff_dur_set(&dev_ctx, 0x06);
     lsm6dso_ff_threshold_set(&dev_ctx, LSM6DSO_FF_TSH_312mg);

    Regards

    Ljian.1
    Ljian.1Author
    Associate
    June 1, 2020

    This is the first time I have used lsm6dso to detect free-fall events. I have not used other ones before.

    I changed the detection threshold to a lower value still not work!

    Ljian.1
    Ljian.1Author
    Associate
    June 1, 2020

    This is my enable free-fall detection sourcecode.

    void static FallDetectionInit(void)

    {

      //stmdev_ctx_t dev_ctx;

      lsm6dso_pin_int1_route_t int1_route;

      /*

      * Uncomment to configure INT 2

      */

      //lsm6dso_pin_int2_route_t int2_route;   

       

      /*

      * Initialize mems driver interface

      */

      //dev_ctx.write_reg = platform_write;

      //dev_ctx.read_reg = platform_read;

       

      /*--------Enable free-fall detection from sensor(lsm6dso)--------*/

      /* Enable LIR */

      lsm6dso_int_notification_set(&dev_ctx, LSM6DSO_ALL_INT_LATCHED);

      /* Set Free Fall duration to 3 and 6 samples event duration */

      lsm6dso_ff_dur_set(&dev_ctx, 0x03);

      lsm6dso_ff_threshold_set(&dev_ctx, LSM6DSO_FF_TSH_312mg);   

       

      /*--------Enable detect activity/inactivity from sensor(lsm6dso)--------*/

      /* Set duration for Activity detection to 9.6 ms (= 4 * 1 / ODR_XL) */

      lsm6dso_wkup_dur_set(&dev_ctx, 0x04);

      /* Set duration for Inactivity detection to 4.92 s (= 4 * 512 / ODR_XL) */

      lsm6dso_act_sleep_dur_set(&dev_ctx, 0x04);

      /* Set Activity/Inactivity threshold to 62.5 mg */

      lsm6dso_wkup_threshold_set(&dev_ctx, 0x02);

       

      /*

      * Inactivity configuration: XL to 12.5 in LP, gyro to Power-Down

      */

      lsm6dso_act_mode_set(&dev_ctx, LSM6DSO_XL_12Hz5_GY_PD);

      /*

      * Enable interrupt generation on Inactivity INT1 pin

      */

      lsm6dso_pin_int1_route_get(&dev_ctx, &int1_route);

      int1_route.md1_cfg.int1_ff = PROPERTY_ENABLE;

      lsm6dso_pin_int1_route_set(&dev_ctx, &int1_route);   

       

       

      /* initialize variables */

      fall_occur = FALL_DETECT_FALSE;

      fall_detect_status = FALL_DETECT_STATUS_NONE;

       

      return;

    }