Skip to main content
AVarg.6
Visitor II
February 14, 2022
Question

Use case: a pressure sensor which acts as an altimeter. At a place where there is a wide season change,does the LPS27HHTW provide the accuracy as mentioned in the Data sheet?My use case has critical implications and need an accuracy of about +1m (.12

Does it also give the mentioned accuracy during weather changes? (Use case is set up in Europe.)

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
February 14, 2022

The datasheet only carries typical values, so no accuracy is guaranteed at all...