Skip to main content
ladislas
Associate II
June 26, 2020
Question

Unico / LSM6DSOX - From decision tree to .ucf (.h) by hand, understanding how .ucf works

Hi there!

​

We've used Unico a lot and find it really cumbersome to create new `.ucf` files: you need to juggle between apps, you can't go back during configuration, if you've made a mistake you have to start from scratch. And it's not possible to automate the process...

​

We've studied the `.ucf` and `.h` files and are wondering how we could generate them without using Unico. Or at least juste use the "copy past the decision tree and generate the files" instead of having to do everything each time.

​

It is possible and if so, where can we find documentation?

Unico is great for evaluation but for our product and use case, it's really not that great.​

​

Thanks a lot!

Ladislas

    This topic has been closed for replies.

    2 replies

    ladislas
    ladislasAuthor
    Associate II
    June 29, 2020

    To be a little more precise:

    When reading a .ucf file, one can quickly notice that the most part is composed of the following commands/registers:

    • 02h - PAGE_SEL
    • 08h - PAGE_ADDRESS
    • 09h - PAGE_VALUE

    For example here, in 4_LSM6DSOX_configuration.ucf:

    Ac 02 11
    Ac 08 EE
    Ac 09 00
    Ac 02 11
    Ac 08 EF
    Ac 09 00
    Ac 02 11
    Ac 08 F0
    Ac 09 0A

    We'd like to understand the mapping of the decision tree:

    F3_VAR_on_ACC_V <= 0.00293
    | F1_MEAN_on_ACC_Z <= -0.844238: face_down (66.0)
    | F1_MEAN_on_ACC_Z > -0.844238: face_up (73.0)
    F3_VAR_on_ACC_V > 0.00293: shaking (51.0)

    To the .ucf.

    We can't seem to find it in the documentation.

    ladislas
    ladislasAuthor
    Associate II
    September 3, 2021

    We still haven't found an answer, any help would be greatly appreciated :)