Skip to main content
Chandu
Associate
July 8, 2019
Question

Unable to load .bin file due to absence of claimed flash memory on STEVAL-IDP005V1.

Hello everyone,

I am trying to load an example .bin file obtained from 'Environmental_Monitoring', an example application present in 'en.stsw-bfa001v1' software package for STEVAL-BFA001V1B predictive maintenance kit. However when I connect the USB cable to the PC, the size of the USB drive is given to be only 32KB (of which only 20KB is free!) whereas the manuals claim the sensor board to have a 2MB flash memory available. The following are the settings applied to the hardware.

  1. Removed JP5(to turn off on board STM32)
  2. Connected the sensor board to the nucleo board via the adapter present in the mentioned kit.

As per the manuals, I have installed the virtual com port driver for windows 10 64-bit and updated the firmware. The following are the manuals I referred to

  1. UM1724
  2. UM0892
  3. UM0627
  4. UM1075
  5. UM2438
  6. STEVAL-BFA001V1 quick started guide

I am powering the STEVAL-IDP005V1 sensor using a DC power supply with voltage set to 20V and the current drawn in around 22mA.

Thanks in advance

-Chandrasekhar DVS

    This topic has been closed for replies.