Skip to main content
Shadab Zafar
Associate
Mar 4, 2018 9:22 AM UTC
Solved

Unable to get SensorTile working

Posted on March 04, 2018 at 10:22

Hello,

I have a SensorTile Kit (STLKT01V1) that I'm trying to test with the Blue MS Android application.

As mentioned in the SensorTile 

http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/bc/b1/ad/c8/36/de/40/92/DM00320099/files/DM00320099.pdf/jcr:content/translations/en.DM00320099.pdf

I plugged in a USB-mini power source but no light blinks on the SensorTile board and the BlueMS app can not find any nearby device.

What am I doing wrong? How can I troubleshoot this?

Thanks.

#sensortile-kit #sensortile
    This topic has been closed for replies.
    Miroslav BATEKBest answer
    ST Employee
    Mar 29, 2018 1:06 PM UTC
    Posted on March 29, 2018 at 15:06

    Did you switch it on?

    Did you upload a firmware?

    4 replies

    santosh23
    Visitor II
    Mar 27, 2018 5:44 PM UTC
    Posted on March 27, 2018 at 19:44

    Hi Zafar,

    Is Orange LED Blinking on the Board ?

    Miroslav BATEKBest answer
    ST Employee
    Mar 29, 2018 1:06 PM UTC
    Posted on March 29, 2018 at 15:06

    Did you switch it on?

    Did you upload a firmware?

    Shadab Zafar
    Associate
    Apr 3, 2018 8:52 AM UTC
    Posted on April 03, 2018 at 08:52

    I realized that by default the kit doesn't have any firmware running. So after connecting it with the Nucleo board and uploading running demo firmwares, things started working!

    Part Robot
    Associate
    Mar 30, 2018 4:26 PM UTC
    Posted on March 30, 2018 at 18:26

    If the BlueCoin is similar, I would imagine it's because of the default firmware the device uses which does not do what you are expecting. To communicate with Blue MS application you must either use the BVLINK firmware (specifically the BVLINK1_ST_Peripheral_8kHz.bin file) or if you want to check out all the features the ALLMEMS1 firmware (I believe the ALLMEMS1_ST_BL.bin file). You will need a Nucleo or something similar (I recommend the NUCLEO-F401RE) to upload this firmware. There's some subtleties getting it all to work which I suspect you'll face, but post back here again if you get stuck and I can help further.