Skip to main content
Associate
Nov 14, 2023 1:29 AM UTC
Question

Ultra Low Power Mode for LSM6DS032 is not working.

Currently designing a  low power embedded system for monitoring application using IMU LSM6DS032, tried both low power/normal mode and the ultra low power mode setting on this IMU, but I could not find the significant difference in the power consumption in these modes.
Any suggestion on the way I am configuring the IMU in ULP mode would be really appreciated.
Steps taken to turning on the Ultra low power mode

  1. Accelerometer is powered-down by setting ODR_[3:0] bits to 0b0000 in CTRL1_XL register.
  2. Gyroscope is powered-down by setting the bits ODR_[3:0] = b0000 of CTRL2_G register.
  3. Setting XL_ULP_EN bit of CTRL5_C to 1.
  4. Setting XL_HM_MODE of CTRL6_C to  0.
  5. Using the FSR of 4G and ODR of 208

Current draw for the MCU interface with IMU is ~2mA  with IMU in ULP/Low-Power mode and MCU in deep sleep. We were expecting draw to be at least in uA range. MCU only deep sleep is ~600uA. Seems like IMU is drawing more than 1mA.

Thank you

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
Nov 17, 2023 10:38 AM UTC

Hi @bimalpaneru ,

Welcome to ST Community!

This is the current consumption reading using LSM6DSO32 with STEVAL-MKI109V3:

FedericaBossi_0-1700217391708.jpeg

However, as you can see reading the datasheet, it is not possible to set ODR 208Hz when you are in ULP mode, so I can't give you a current consumption values.

In addition, when you set to '0' xl_hp mode, you enable the HP mode:

FedericaBossi_1-1700217487331.jpeg

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
Jan 17, 2024 3:52 AM UTC

Hi @Federica Bossi ,

Thank you for you reply.
Can you please clarify on these?
Datasheet says for ULP mode for ODR_XL between 1.6 Hz and 208 Hz possible. Is this a open range rather than closed?

Also, the application note section 3.5 mentions Six low-speed ODRs can be chosen for the accelerometer through the ODR_XL bits: 1.6 Hz, 12.5 Hz,26 Hz, 52 Hz, 104 Hz, and 208 Hz. The gyroscope must be set in power-down mode.


And, section 6.2.1 of datasheet says, When ULP mode is intended to be used, the bit XL_HM_MODE must be set to 0, which turns the HP mode on. Does this bit have to be '1' for ULP mode?


Associate
Aug 7, 2025 5:26 PM UTC

Hi @Federica Bossi 

Following up for this clarification. 

Thanks