Skip to main content
Evelina CAMILLERI
ST Employee
Nov 11, 2022 1:56 PM UTC
Solved

Thinking about 9-axis sensor fusion: can ISPU core take in sensor raw data in periphery and real-time fusing more accurate orientation information?

..

    This topic has been closed for replies.
    Luca SEGHIZZI
    Luca SEGHIZZIBest answer
    Senior
    Nov 11, 2022 2:22 PM UTC

    Yes, with the ISPU we can use the sensor hub configuration using up to 4 sensors, hence yes, we can take the magnetometer and compute the 9-axis sensor fusion with a total power consumption of 370uA.

    2 replies

    Luca SEGHIZZI
    Luca SEGHIZZIBest answer
    Senior
    Nov 11, 2022 2:22 PM UTC

    Yes, with the ISPU we can use the sensor hub configuration using up to 4 sensors, hence yes, we can take the magnetometer and compute the 9-axis sensor fusion with a total power consumption of 370uA.

    Associate
    Apr 16, 2024 10:24 AM UTC
    Hi, I would like to use LSM6DSO16IS+LIS2MDL,LIS2MDL is mounted via the sensor hub on the LSM6DSO16IS,The ISPU function outputs quaternion data. I went through the relevant package(en.x-cube-ispu),But I still don't understand how the 9 axis sensor fusion application should be configured.
    Is there a simple ISPU code related to acc + gro + mag?