Skip to main content
6June.1
Associate II
Feb 1, 2021 10:34 AM UTC
Solved

The ID value read by ism330dhcx chip is always 0

Hi, st

The MCU platform I use is nrf52840. The sensor uses steval-mki207v1. The hardware connection method is mode 1. The SPI mode of MCU is mode0, the frequency is 8MHz, and the bit order is MSB first.

On this premise, no matter how many times I read the chip ID, the value is 0.What is the problem?

    This topic has been closed for replies.
    6June.1
    6June.1Best answer
    Associate II
    Feb 1, 2021 12:28 PM UTC

    Is the MCU platform SPI operation error problem, now has solved, Thanks�?

    5 replies

    6June.1
    6June.1AuthorBest answer
    Associate II
    Feb 1, 2021 12:28 PM UTC

    Is the MCU platform SPI operation error problem, now has solved, Thanks�?

    Eleon BORLINI
    ST Employee
    Feb 1, 2021 2:31 PM UTC

    Hi @6June.1​ ,

    glad to hear it and happy you reported you found the solution!

    -Eleon

    6June.1
    6June.1Author
    Associate II
    Feb 2, 2021 9:58 AM UTC

    Hi, Eleon BORLINI

    Now I've found some new problems.

    ​

    Sometimes the value read from who AMI register will be 0x48. After finding this problem, I suspect that the connecting wire is unstable. After replacing the DuPont wire, the value read back to normal (0x6b). I want to ask what is the reason for this strange phenomenon.

    In addition, I found that the accelerometer data rate can only be set at 833hz or below. If the accelerometer data rate is set above 1667hz (16673hz,3333hz,6667hz), the value read from the register is still the previous value, that is, the data setting above 1667hz always fails.

    ​

    So I updated the driver file to the version of 5 days ago (ism330dhcx: fixed examples # 107) in Git library.

    A step was added to the driver calling routine of this version(ism330dhcx_device_conf_set), but this step didn't seem to succeed.

    After execution, I also read the value of this register(ism330dhcx_device_conf_get(&dev_ctx, &rst)), and the returned value is 0(rst == 0).

    In other words, the device_conf bit is not really set to 1 and remains in the default state after the set is executed.

    But according to the datasheet, it seems that this bit must be set to 1 to write the new configuration normally?

    Now I'm a little confused, can you help me answer the three questions of appeal?

    Eleon BORLINI
    ST Employee
    Feb 2, 2021 1:20 PM UTC

    Hi @6June.1​ ,

    I saw you added a new question here.

    I'll respond to that one and close this thread.

    -Eleon