Skip to main content
MWaqa.2
Visitor II
April 19, 2021
Question

The attractive sensor of STEVAL-MKI173V doesn't enter the information prepared state by I2C correspondence.

Composed 0x40 to the CTRL1_A register, composed 0x8C to the CFG_REG_A_M register. 

I had the option to peruse the information on the accelerometer by means of I2C correspondence, however the attractive sensor can't understand it. 

How would I change the "Zyxda" bit in the attractive sensor's STATUS_REG_M to 1? 

If it's not too much trouble, advise me. 

Upon assessment, I tracked down that the "Zyxda" piece of the attractive sensor's STATUS_REG_M didn't get 1. 

There was no mistake in the I2C correspondence itself. 

Furthermore, I2C correspondence was performed by the correspondence arrangement of LSM303AH.

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
April 19, 2021

Hi @Community member​ ,

to check if the I2C is fully operating (assuming the digital pattern is correct and you are receiving the ACK from the slave), did you try to read the WHO_AM_I registers of both accelerometer and magnetometer?

If so, you can check from this C driver on Github (lsm303ah_read_data_polling.c) if you correctly configuring the sensor:

/* Enable Block Data Update */
 lsm303ah_xl_block_data_update_set(&dev_ctx_xl, PROPERTY_ENABLE);
 lsm303ah_mg_block_data_update_set(&dev_ctx_mg, PROPERTY_ENABLE);
/* Set full scale */
 lsm303ah_xl_full_scale_set(&dev_ctx_xl, LSM303AH_XL_2g);
/* Set / Reset magnetic sensor mode */
 lsm303ah_mg_set_rst_mode_set(&dev_ctx_mg,
 LSM303AH_MG_SENS_OFF_CANC_EVERY_ODR);
/* Enable temperature compensation on mag sensor */
 lsm303ah_mg_offset_temp_comp_set(&dev_ctx_mg, PROPERTY_ENABLE);
/* Set Output Data Rate */
 lsm303ah_xl_data_rate_set(&dev_ctx_xl, LSM303AH_XL_ODR_100Hz_LP);
 lsm303ah_mg_data_rate_set(&dev_ctx_mg, LSM303AH_MG_ODR_10Hz);
/* Set magnetometer in continuous mode */
 lsm303ah_mg_operating_mode_set(&dev_ctx_mg,
 LSM303AH_MG_CONTINUOUS_MODE);

-Eleon