Skip to main content
SS_135
Associate
September 3, 2020
Question

Support for Unicleo-GUI

Hi Team,

Dear Team

Gone through the user manual, refer the below link

https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/b9/d0/7c/c5/a8/55/4c/bc/DM00337036/files/DM00337036.pdf/jcr:content/translations/en.DM00337036.pdf

Also find the below part used

MCU : STM32F446RE

Accelerometer : ISM330DLC

Microphone: MP34DT06

Actually able to port vibration sensor FFT data to Unicleo-GUI, and able to port microphone sensor FFT data to Unicleo-GUI. 

The challenge what we are facing is, we are not able to port both vibration sensor and microphone sensor FFT data to Unicleo-GUI. 

Please let us know if you have a test application or reference source code to port both vibration sensor and microphone sensor FFT data to Unicleo-GUI.

Regards

Sudeendra S​

    This topic has been closed for replies.

    6 replies

    SS_135
    SS_135Author
    Associate
    September 7, 2020

    Dear Eleon,

    Thanks for the reply. Actually, customer referred Vibration Monitoring and Microphone FFT from X-CUBE-MEMS1.

    The challenge is the Unicleo-GUI does not support both Vibration Monitoring and Microphone FFT at the same time

    Do you have a reference code where both shall be represented at same time.Please do the needfull.

    Regards

    Sudeendra S

    Eleon BORLINI
    ST Employee
    September 11, 2020

    Hi @SS_135​ ,

    I double-checked with our Unicleo experts and I confirm you that unfortunately the Unicleo-GUI doesn’t support displaying both vibration and microphone FFT data in any mode. It is designed to support individual example application (it is conceived mostly for demo applications) so there is no way to display all data he requested at the same time in Unicleo-GUI.

    I suppose you should manage the "simultaneous" acquisition of the vibration signal and the audio signal at firmware level: you could try to integrate the two FW libraries in your own project, initializing the IMU and microphone peripheral (SPI and I2S/PDM) for the acquisitions together and calculate the two FFT in DMA. If you need more support, you can ask to an ST representative from your geographical area at this link.

    -Eleon