Skip to main content
NMale.1
Associate II
Oct 28, 2020 9:26 AM UTC
Solved

Suggest me an accelerometer sensor for speed calculation of moving vehicle.Dynamic values of an accelerometer.

I want to use an accelerometer to calculate the speed of a moving vehicle. For this i need a accelerometer which should give _ve values(2's complement) in Deceleration and +ve values in (2's complement) in acceleration. It should have 2g range with 12bit(or more) resolution. with less noise affected. It should have less Zero offset error.

If there is any sensor Please Suggest me one.

Thank you in Advance.

This topic has been closed for replies.
Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Oct 28, 2020 10:01 AM UTC

Hi @NMale.1​ ,

connecting this post to this thread.

One of the accelerometers with low noise available in ST portfolio is the LIS2DW12, that can operate in high performance mode, 14-bit, with about 100 ug/sqrt(Hz) noise.

I suggest you to compensate an eventual residual initial offset acting on X_OFS_USR (3Ch) to Z_OFS_USR (3Eh) registers.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
Oct 28, 2020 10:01 AM UTC

Hi @NMale.1​ ,

connecting this post to this thread.

One of the accelerometers with low noise available in ST portfolio is the LIS2DW12, that can operate in high performance mode, 14-bit, with about 100 ug/sqrt(Hz) noise.

I suggest you to compensate an eventual residual initial offset acting on X_OFS_USR (3Ch) to Z_OFS_USR (3Eh) registers.

-Eleon