Skip to main content
Visitor II
August 18, 2023
Question

STWINKT 1B bug in fft analys demo.

In ultrasoun library has a bug. If change you in fft_app.h FFT_OUTPUT program is not compiled. Please change code like this

 

 

static void FFT_Thread(void const *argument)
{
 (void) argument;

#if (configUSE_APPLICATION_TASK_TAG == 1 && defined(TASK_FFT_DEBUG_PIN))
 vTaskSetApplicationTaskTag(NULL, (TaskHookFunction_t)TASK_FFT_DEBUG_PIN);
#endif

#ifdef DATA_TEST
 static uint16_t usbTestData = 0;
#endif

#if (FFT_OUTPUT == FFT_AVERAGE)
 uint16_t nAccTotal = 10;
 uint16_t nAcc = 0;
#endif

 FFT_Lib_Init(512, 0.5f);

 for (;;)
 {
 osSemaphoreWait(fft_data_input_sem_id, osWaitForever);
 FFT_Process(&audio_fft_instance, audio_fft_out);

#if (FFT_OUTPUT == FFT_RAW)
 if (com_status == HS_DATALOG_USB_STARTED)
 {
 USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *) audio_fft_out,
 sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
 }
#elif (FFT_OUTPUT == FFT_AVERAGE)
 arm_add_f32(audio_fft_out, FFT_Average, FFT_Average, audio_fft_instance.init_params.FFT_len / 2);
 nAcc++;

 if (nAcc == nAccTotal)
 {
 arm_scale_f32(FFT_Average, 1.0f / (float)nAcc, FFT_Average, audio_fft_instance.init_params.FFT_len / 2);
 if (com_status == HS_DATALOG_USB_STARTED)
 {
 USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *)FFT_Average,
 sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
 }
 memset((uint8_t *)FFT_Average, 0, audio_fft_instance.init_params.FFT_len / 2);
 nAcc = 0;
 }
#elif (FFT_OUTPUT == FFT_WEIGHTED_AVERAGE)
 uint32_t i;
 for (i = 0; i < audio_fft_instance.init_params.FFT_len / 2; i++)
 {
 audio_fft_out[i] = FFT_Average[i] * 0.97f + audio_fft_out[i] * 0.03f;
 FFT_Average[i] = audio_fft_out[i];
 }
 if (com_status == HS_DATALOG_USB_STARTED)
 {
 USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *)FFT_Average,
 sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
 }
#endif

#ifdef DATA_TEST
 uint16_t i = 0;

 int16_t *p16 = (int16_t *)dataOut;
 for (i = 0; i < 4; i++)
 {
 *p16++ = usbTestData++;
 }
#endif
 }
}

 

    This topic has been closed for replies.

    1 reply

    niccolò
    ST Employee
    August 21, 2023

    Hi @karakasali ,

    Welcome to ST community =)

    thank you for your input, but would you mind explaining what is the problem with the default library?

    Niccolò