Skip to main content
HMajc.1
Associate
December 8, 2022
Solved

STM32H743ZIT6 (NUCLEO-H743ZI) not compatible with the expansion board X-NUCLEO-CCA02M2?

I wanna do a live audio processing project and I got an X-NUCLEO-CCA02M2 expansion board with the integrated mics as it says it's compatible with all STM32 boards. However, the pins seem misaligned, i.e. i can't just plug it nicely on top as shown in the manuals or tutorials. Am I missing something? Is there some nonstandard way of connecting those two particular modules together?

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
December 12, 2022

Hello @HMaje.1​,

To connect an X-NUCLEO-CCA02M2 expansion board to a NUCLEO-F746ZG for example development board, morpho header connectors must be soldered on the relevant footprint available on the STM32 Nucleo.

Also, you do not need to solder the whole 2 x 80 pin header but only a pair of 2 x 38 pin stripline connectors as mentioned in Getting started with the digital MEMS microphone expansion board based on MP34DT06J for STM32 Nucleo - User manual  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

FBLBest answer
ST Technical Moderator
December 12, 2022

Hello @HMaje.1​,

To connect an X-NUCLEO-CCA02M2 expansion board to a NUCLEO-F746ZG for example development board, morpho header connectors must be soldered on the relevant footprint available on the STM32 Nucleo.

Also, you do not need to solder the whole 2 x 80 pin header but only a pair of 2 x 38 pin stripline connectors as mentioned in Getting started with the digital MEMS microphone expansion board based on MP34DT06J for STM32 Nucleo - User manual  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
HMajc.1
HMajc.1Author
Associate
December 13, 2022

Oh, I see, that's unfortunate.

Thank you for a quick response, I'll refer to the materials provided.

Best,

Hubert