Skip to main content
TPhil.3
Associate
Apr 14, 2025 7:59 PM UTC
Solved

STHS34PF80TR INT pin Source / Sink capability?

Greetings - what are the recommended maximum current ratings for the INT pin in either Push-Pull or Open-Drain? And FWIW, I was really surprised NOT to find this published in the datasheet...

TIA,

-Terry

This topic has been closed for replies.
Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Apr 18, 2025 1:25 PM UTC

Hi @TPhil.3 ,

The interrupt pin can sink maximum 4mA.

Consider that the interrupt pins are usually connected directly to a microcontroller and are not made to drive load (e.g., LEDs).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Apr 18, 2025 1:25 PM UTC

Hi @TPhil.3 ,

The interrupt pin can sink maximum 4mA.

Consider that the interrupt pins are usually connected directly to a microcontroller and are not made to drive load (e.g., LEDs).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.