Associate
October 26, 2016
Question
STEVAL WESU1 understanding logged data
- 2 replies
- 1008 views
Posted on October 26, 2016 at 16:43
Hi ,
I have STEVAL WESU module and logged acelerometer data using android app. (plz see attached file)My settings are: Timer: 512 Hz, 10Hz, 1HzMEMS Accelerometer output data rate: 416 Hz , 833 Hz, 100HzIn the logged data host time stamps and node time stamps are available. My observation:All the time stamps are in milliseconds.Host, stamp time on data at 100Hz if Timer value > 100Hz otherwise at Timer value. Node, stamp time on data at 1000Hz irrespective of ''MEMS Accelerometer output data rate'' settings. If Host time stamp rate lower than node time stamp, then are we losing data? What is allowable max. data rate at which we can log accelerometer data considering BLE protocol? As per sensor data sheet 1Hz- few kHz data rate is allowed. thank you, #steval-wesu