Skip to main content
Associate II
Feb 27, 2024 3:10 PM UTC
Question

STEVAL-STWINBX1 cloud logging

Hello,

I have a requirement to log the data from evaluation board STEVAL-STWINBX1 to cloud. I have created Azure IOT hub and while initiating the cloud logging from the app i was unable to successfully connect to the created IOT Device created in azure even though the connection string was pasted correctly. the application ST BLE Sensor classic automatically disconnects from the sensor once the cloud logging is enabled. do i need to install the SD card and log the data from card to cloud ? I got struck at this point, is there any specific firmware to be loaded, for now I'm just testing with the basic firmware that provides data from all the sensors to the app

3 replies

Associate II
Nov 7, 2025 1:21 PM UTC

Hi Dinesh I am also working on a similar project in which i have to condition monitor the wind turbine blade acoustic signals. i would like to know if you have found out the soultion for your problem

kind regards
Jose John

Associate II
Nov 8, 2025 12:34 AM UTC

Hello Jose,

 

yes, I was able to connect to the ST cloud but finally settled with Bluetooth communication developing the entire application with Flutter Ble Plus paired with Ble gateway which can push the data back to cloud, let me know if you want to implement something similar.

 

Regards

Dinesh Kumar

Associate II
Nov 10, 2025 12:17 PM UTC

Hi Dinesh, Thankyou so much for your reply. i would also like to do the same with WIFI, as the box has a  inbuilt WIFI module. As of now would please let me know how did you set up the cloud backup. I really appreciate your help in this as i have not received any reply from community since i posted about this topic. you can also connect to me via LinkedIn (https://www.linkedin.com/in/josejohna).

Kind regards 
Jose John