Skip to main content
Visitor II
May 16, 2025 5:35 PM UTC
Question

STEVAL-STLKT01V1

Good morning, I am programming a SensorTile using the STEVAL-STLKT01V1 expansion kit, and when I flash the program to the device, I encounter the following error:
Break at address "0x8000270" with no debug information available, or outside of program code.

This topic has been closed for replies.

2 replies

SimonePradolini
ST Technical Moderator
May 19, 2025 8:30 AM UTC

Hello @luca12017 

How did you flashed the board? Are you using STM32CubeProgrammer? It seems an issue with the address or the bank of the flash. You can check the start address: it should be 0x08000000 in a firwmare without bootloader.

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SimonePradolini
ST Technical Moderator
Jun 19, 2025 10:00 AM UTC

Hello @luca12017 

Any news on the topic? Did you flashed the board successfully?

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.