Skip to main content
KDług.1
Associate
February 10, 2023
Question

STEVAL-MKI208V1K conecting to nucleo F401

Hello I want to connect to the STEVAL-MKI208V1K via STEVAL-MKIGIBV2 (conected those both togheter) , with Nucleo-F401RE. I conected pins as it is shown below

F401RE-> MKIGIBV2

MOSI (PB3 -> SDA

MISO -> SDO

SCK -> SCL

PWM/D6 -> CS

3v3 -> VDD

GND- >GND

I want to use SPI 4 wire interface but immediately after connecting nucleo to the PC I lost conection to the board and led LD1 starts blinking red. Do I need to connect some other pins as well with a board? Do I need to use some pull up resistors to the pins?

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    ST Technical Moderator
    April 12, 2023

    Hi @Konrad Długozima​ ,

    You need to connect also VDDIO to 3V3.

    Let me know if this solve your problem and in case please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.