Question
STEVAL-MKBOXPRO firmware that is compatible with ISPU dil24
- 1 reply
- 1043 views
I'm trying to make a demo with the ispu chip ism330is and the STEVAL-MKBOXPRO the issue is I can't find a suitable firmware for the tilebox pro that is compatible with the ispu and allows me upload the compiled UCF program into the chip. Below is a screenshot of the current firmware I'm using FPSNS DATALOG 2 in which it shows the ispu as unknown and if I try to upload the UCF it's just gets stuck!