Skip to main content
DRote.2297
Associate II
May 9, 2020
Question

SPI not working with LSM6DSL

Hello,

I'm using NUCLEO-L476RG connected to eval board of LSM6DSL. I have checked the physical connection with a DVM and it seems to be correct.

I have generated a very simple project using STM32CubeIDE and trying to read the WHO_AM_I register (code below). I'm using a simple USB logic analyzer and I can see that the data is being output correctly on the MOSI line, but there is no answer on the MISO line. What am I missing here?

uint8_t who_am_I; // Who Am I
who_am_I |= 0x0f;
 
while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
	 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
	 HAL_GPIO_WritePin(SPI1_nCS_GPIO_Port, SPI1_nCS_Pin, GPIO_PIN_RESET); //Set SPI CS to low
	 HAL_SPI_Transmit(&hspi1, &who_am_I, 1, 1000); // Read Who Am I register
	 while(HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
	 HAL_SPI_Receive(&hspi1, &pBuffer, 1, 1000);
 
//	 HAL_SPI_TransmitReceive(&hspi1, &who_am_I, &pBuffer, who_am_I, 1000);
 
	 HAL_GPIO_WritePin(SPI1_nCS_GPIO_Port, SPI1_nCS_Pin, GPIO_PIN_SET); //Set SPI CS to high
 
 
	 HAL_Delay(100);
	 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
	 HAL_Delay(100);
 }

This topic has been closed for replies.

2 replies

Eleon BORLINI
ST Employee
May 11, 2020

Hi @DRote.2297​ , can you check the MISO and MOSI line with an oscilloscope, if you are getting something like 00h or FFh? Btw, I suggest you to check the STM32CubeL4 firmware package, both in the folder \Drivers\BSP\Components\lsm6dsl, which contains the LSM6DSL drivers for the STM32L4 MCU family and the folder \Projects\NUCLEO-L476RG\Examples\SPI for checking the correct SPI initialization on NUCLEO L4 platform. Regards

DRote.2297
Associate II
May 11, 2020

Hi @Eleon BORLINI​ , unfortunately I don't have an oscilloscope. I have a USB logic analyzer - when I use it I see FFh.

I initiated the SPI using STM32CubeIDE, tried few different SPI configurations but the result is always the same. What else can it be?