Skip to main content
Associate
May 4, 2026 6:40 AM UTC
Question

Sound measurement with very steep gradient

We have been using the ST MP23DB01HP microphone to measure the shockwave signature of assault rifles. When comparing the time signal with measurements performed with other microphones (e.g. B&K model 4948), we noticed that the typical N-wave signature looks different with the ST microphone. The initial compression wave of the shock appears negative when measured with the ST microphone, which is counter intuitive. Also, the expansion phase of the shockwave, which appears relatively clean when measured with the B&K microphone, is severely perturbed when measured with the ST microphone. Could it be that the perturbation observed with the ST microphone is of internal nature, e.g. caused by some internal flow due to the shockwave and not properly vented out of the casing? What other possible causes would you see? Exceeded acoustic overload point? Tthe shockwave has very strong gradients, that might interact negatively with the ST microphone.

2 replies

Federica Bossi
ST Technical Moderator
Jun 15, 2026 9:32 AM UTC

Hi ​@thmaeder ,

Could you please provide the shock level measured with the B&K system? Since the MP23DB01HP has an acoustic overload point of 135 dBSPL, while the B&K microphone reaches 160 dBSPL, it is therefore possible that the applied level is beyond the usable range of the MP23DB01HP.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
thmaederAuthor
Associate
Jun 16, 2026 7:10 AM UTC

Hello ​@Federica Bossi ,

the level was about the 135 dB AOP. What happens to the MP23DB01HP microphone when it has to deal with sound level on the order of 150-160 dB? Is there a typical behavior? Or is it random?