Skip to main content
irene
Associate II
September 24, 2019
Solved

(SOLVED) SPI communication problem with sensors

I'm using STEVAL-STWINKT1 (MCU STM32L4R9ZIJ6) and I'm trying to communicate with the motion sensors (ISM330DHCX, IIS3DWB, IIS2DH) by SPI3 interface (polling). I wrote a code very similar to that one present in the "Serial_DataLog" project, using HALs (I'm using STM32CubeIDE and STM32CubeMX generated code). I'm trying to get the WHO_AM_I value from register address 0x0F, but my code gives me cyclically a wrong value every time I call this function.

Here it is my code:

- in main.c

static void MX_SPI3_Init(void)
{
 
 /* USER CODE BEGIN SPI3_Init 0 */
 
 /* USER CODE END SPI3_Init 0 */
 
 /* USER CODE BEGIN SPI3_Init 1 */
 
 /* USER CODE END SPI3_Init 1 */
 /* SPI3 parameter configuration*/
 hspi3.Instance = SPI3;
 hspi3.Init.Mode = SPI_MODE_MASTER;
 hspi3.Init.Direction = SPI_DIRECTION_2LINES;
 hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi3.Init.CLKPolarity = SPI_POLARITY_HIGH;
 hspi3.Init.CLKPhase = SPI_PHASE_2EDGE;
 hspi3.Init.NSS = SPI_NSS_SOFT;
 hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
 hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi3.Init.CRCPolynomial = 7;
 hspi3.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi3.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI3_Init 2 */
 __HAL_SPI_ENABLE(&hspi3);
 /* USER CODE END SPI3_Init 2 */
 
}

- in sensor_bsp.c

#include "stm32l4xx_hal.h"
#include "vibro.h"
#include "main.h"
#include "stm32l4xx_hal_spi.h"
 
extern SPI_HandleTypeDef hspi3;
 
/* #define + typedef */
#define TIMEOUT_DURATION			1000u				
#define VIBRO_CS_GPIO_CLK_ENABLE()	__GPIOF_CLK_ENABLE()
GPIO_InitTypeDef GPIO_InitStruct;
 
#define SPI3_SIZE	SPI_DATASIZE_8BIT
 
/* register addresses */
#define VIBRO_SENSE_REG_MANID 	0x0Fu
 
/* private functions */
static HAL_StatusTypeDef VIBRO_SPI3_Send(uint8_t *pdata, uint16_t len);
static HAL_StatusTypeDef VIBRO_SPI3_Receive(uint8_t *pdata, uint16_t len);
static HAL_StatusTypeDef VIBRO_SPI3_ReadReg(uint16_t Reg, uint8_t *pdata, uint16_t len);
 
/* public functions (impl) */
void VIBRO_Init(void)
{
 /* Peripheral clock enable */
	__HAL_RCC_SPI3_CLK_ENABLE();
	/**SPI3 GPIO Configuration
	PB4 (NJTRST) 		 ------> SPI3_MISO
	PB5 				 ------> SPI3_MOSI
	PB3 (JTDO/TRACESWO) ------> SPI3_SCK
	*/
	GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_3;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
	GPIO_InitStruct.Alternate = GPIO_AF6_SPI3;
	HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
			
	__GPIOF_CLK_ENABLE();
	GPIO_InitStruct.Pin = CS_ADWB_Pin;
	HAL_GPIO_Init(CS_ADWB_GPIO_Port, &GPIO_InitStruct);
	
	/* Configure ISM330DHC pin */
	HAL_GPIO_WritePin(CS_DHC_GPIO_Port, CS_DHC_Pin, GPIO_PIN_SET); 
}
 
 
HAL_StatusTypeDef VIBRO_ReadManID(uint8_t* manId)
{
	return VIBRO_SPI3_ReadReg(VIBRO_SENSE_REG_MANID, manId, 0x01u);
}
 
/* private functions (impl) */
static HAL_StatusTypeDef VIBRO_SPI3_Send(uint8_t* pdata, uint16_t len)
{
	return HAL_SPI_Transmit(&hspi3, pdata, len, TIMEOUT_DURATION);
}
 
static HAL_StatusTypeDef VIBRO_SPI3_Receive(uint8_t* pdata, uint16_t len)
{
	return HAL_SPI_Receive(&hspi3, pdata, len, TIMEOUT_DURATION);
}
 
 
static HAL_StatusTypeDef VIBRO_SPI3_ReadReg(uint16_t Reg, uint8_t* pdata, uint16_t len)
{
	uint8_t dataReg = (uint8_t)Reg;
	dataReg |= 0x80U;
	
	HAL_StatusTypeDef retval = HAL_OK;
 
	/* 1 select slave */
	HAL_GPIO_WritePin(CS_DHC_GPIO_Port, CS_DHC_Pin, GPIO_PIN_RESET);
 
	/* 2 do transaction */
	 if (VIBRO_SPI3_Send(&dataReg, 1) != HAL_OK)
	 {
		retval = HAL_ERROR;
	 }
 
	 if (VIBRO_SPI3_Receive(pdata, len) != HAL_OK)
	 {
		retval = HAL_ERROR;
	 }
	/* 3 de-select slave */
	HAL_GPIO_WritePin(CS_DHC_GPIO_Port, CS_DHC_Pin, GPIO_PIN_SET);
 
	return retval;
}

I tried also with a different SPI3 initialization CLK polarity and phase, but the result is the same as before:

 hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;

 hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;

What's the problem?

P.S.: I don't really understand the command dataReg |= 0x80U. I looked up at the sensor datasheet and I didn't find this info: where'd that come from?

P.P.S.: I checked the pinout and it's correct.

This topic has been closed for replies.
Bill Dempsey
Bill DempseyBest answer
Associate III
September 26, 2019

Bit7 is NOT for multi-read but for READ. Multibyte is bit6, The target device does not know if you are reading or writing its register without setting bit7 appropriately. The SPI interface and bits are described in detail in the datasheets.

I believe your initial code polarity and phase are right but check with an oscillscope. Perhaps add some additional debug messages throughout the code to solve this issue. The general concept looks correct.

7 replies

S.Ma
Principal
September 24, 2019

The 0x80 (bit 7 set) is usually for multi-byte read/write: If the bit is set, you read registers in incremental address. Otherwise, you keep reading the same register (for example waiting for a flag to be set).

irene
ireneAuthor
Associate II
September 25, 2019

Understood. After a deep reading of the sensors datasheets I found the point "bit 0: READ bit. The value is 1.", that corresponds to 80h.

S.Ma
Principal
September 24, 2019

Some mems in SPI mode boot in 4 wire, others in 3 wire mode.

irene
ireneAuthor
Associate II
September 25, 2019

And so, according to my problem, what's the point?

Visitor II
October 6, 2023

Hello, I'm also using the IIS2DH sensor, and I'm getting the same error you're getting. Can you share your code? Thank you.