Skip to main content
Associate
April 23, 2024
Question

Software compatibility of LSM6DSV32X with previous IMU products

I need to have a part that goes beyond +/-2000 dps.  The new part LSM6DSV32X does just that (4000 dps).  I'm hoping that it is software/register compatible with the LSM6DSO line of IMUs.  That way I could just replace this part (pin compatible) and update the register for the range of the gyro and leave the remaining code the same.    

Is that true?  Can I do this?

This topic has been closed for replies.

7 replies

Federica Bossi
ST Technical Moderator
April 24, 2024

Hi @DaveD ,

Welcome to ST Community!

It depends on which registers you are using. You could look on the datasheet to see if they have remained the same or changed.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
DaveDAuthor
Associate
April 24, 2024

The data sheet has 200 pages to it so that is a rather large effort to compare this part to others in its family of parts.  Other manufacturers often have a section in their data sheets (or an app note) that explain the differences between parts in a family to allow a design engineer to avoid putting in extensive amounts of time on something that is already known by the manufacturer.    Would it be possible to have the product manager write up what the differences are in the register set?

 

DaveDAuthor
Associate
April 24, 2024

To be more specific, we already had an application where we moved from a LSM6DSO to an LSM6DSO32 and there were bugs in the ST provided driver that cost us a huge amount of time.  I will try to go back into my archives to be more specific regarding the details on this past history but it is an "existence proof" that i could be signing myself up for another huge problem. 

My goal is to see if there is a possibility that the register incompatibilities are a non-issue and I could use the same driver I have with the exception of writing the register to change the range of the gyro.

Any information you could provide on the product could save hours of design time.

thanks,

dave

 

Federica Bossi
ST Technical Moderator
May 2, 2024

Hi @DaveD ,

They are two different products and so there are obviously differences. I can try to help you if you give me more details about your application and what driver you are using. Also are you only interested in the differences for the accelerometer?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
DaveDAuthor
Associate
May 2, 2024

Here is the situation I am trying to resolve.

The LSM6DSO works fine in our application with the exception that the 2Kdps gyro range sometimes saturates.  If the identical part existed with a 4Kdps the design would work perfectly.

 

The hopeful solution would be to upgrade to the LSM6DSO32 since it has 4Kdps range.  I need no other new features from it in order to be successful.  I am uninterested in any other new features at this point in time other than the increased range of the gyro.

 

So, my question is, can I use my updated/fixed LSM6DSO driver with an LSM6DSO32 (with the only modification being to change the gyro range) and have a drop in replacement.

Any help in answering this question would be appreciated.

dave

Federica Bossi
ST Technical Moderator
May 2, 2024

Hi @DaveD ,

I don't understand if you want to use an LSM6DSV32X (as written in the first message) or LSM6DSO32.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.