Skip to main content
Associate
May 17, 2024
Question

SensorTileBox Pro recognizes steval-mki197v1 as LSM6DSO32

Hi there, 

In the app, my steval-mki197v1 with LSM6dsox gets recognized as LAM6DSO32.

Is this normal behaviour?

luika

This topic has been closed for replies.

5 replies

Federica Bossi
ST Technical Moderator
May 21, 2024

Hi @luik ,

Welcome to ST Community!

Unfortunately LSM6DSOX is not supported, on the contrary LSM6DSO32X is. For this reason it is probably misread.
The possibility of using STEVAL-MKI197V1 will certainly be added in the future.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
luikAuthor
Associate
May 21, 2024

Apart from being labeled wrong, it seems to work just fine but i did no further testing. Is it maybe compatible and useable?

Federica Bossi
ST Technical Moderator
May 23, 2024

Hi @luik ,

The two sensors are similar but not the same, so it may be that for the registers you are looking at it works but we do not guarantee it for all features. The device that is currently supported is only LSM6DSO32X.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
luikAuthor
Associate
May 27, 2024

Thank you for the answer.
The STEVAL MKI229AA features the LSM6DSO16IS IMU.

Is the data of the LSM6DSO16IS compareable to a LSM6DSOX?

They both feature the same sampling rates and scales.

Best regards,

Luis

 

Federica Bossi
ST Technical Moderator
May 28, 2024

Hi @luik ,

Do you mean if you could use the LSM6DSOIS instead of LSM6DSOX?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.