Skip to main content
Am1
Visitor II
Jul 4, 2019 11:01 PM UTC
Solved

SensorTile.box schematics

Hi,

I have a SensorTile.box from ST. But unfortunately there is no board schematics in the product resources part! I appreciate if some one help and let me know about it.

Kind regards

    This topic has been closed for replies.
    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Aug 2, 2019 11:48 AM UTC

    Glad to inform you that the SensorTile.box block diagram and schematics are now available online --> link

    Regards

    7 replies

    Eleon BORLINI
    ST Employee
    Jul 5, 2019 7:28 AM UTC

    ​Hi @Am​ ​, the schematics will be soon available on st.com (I hope in a couple of weeks). It's not available by now due to some cosmetic changes. Regards

    RafaelJoseph
    Associate II
    Jul 24, 2019 6:10 AM UTC

    Hi

    Any update on this?

    thanks!

    Eleon BORLINI
    ST Employee
    Jul 24, 2019 12:05 PM UTC

    HI @RafaelJoseph​ , unfortunately not yet, but should be soon ready. My two-weeks hypothesis was too optimistic, cause I did't take into account the vacation period. Sorry for the delay. Regards

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    Aug 2, 2019 11:48 AM UTC

    Glad to inform you that the SensorTile.box block diagram and schematics are now available online --> link

    Regards

    RafaelJoseph
    Associate II
    Aug 2, 2019 12:00 PM UTC

    Thanks for the update!

    AKato.1
    Associate
    Jun 4, 2020 8:33 AM UTC

    I was wondering, if the SensorTile.box block diagram and schematics (link) are correct. If I am not mistaken it should contain a LSM6DSOX sensor, which is connected through SPI1. (My statements are based on the code generated by Algobuilder.)

    Best regards,

    Attila

    Eleon BORLINI
    ST Employee
    Jun 4, 2020 8:51 AM UTC

    Hi @AKato.1​ , you are right, the IMU sensor on the ST.box is a LSM6DSOX and not a LSM6DSO. There is a mistake on the schematic... Regards