Skip to main content
Associate II
November 3, 2023
Question

SensorTile.box PRO project in STM32CubeIDE from scratch

 

Hello. I would like to make a new project for the "SensorTile.box PRO" board using STM32CubeIDE. It appears that the board is not available. (In the image below, you can see that I have filtered on "box" and only the non-pro SensorTile.box device shows up. These two boards are quite different (MCU, peripherals, etc.) so I can't use it.

Is this a bug or omission in the tool? Do I need to add the SensorTile.box PRO BSP manually or something?

Thanks

stuart_rubin_ns_0-1699030180133.png

 

This topic has been closed for replies.