Skip to main content
Associate
December 17, 2024
Question

SensorTile.box Lost Power, Connection

I just bought the latest SensorTileBox (STEVAL-MKSBOX1V1) and it lost power and bluetooth connection, no LED lights. How do I restore it to its original firmware? The ST BLE Sensor app also doesn't have the create app option.

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
December 20, 2024

Hi @tortilla ,

Here the steps to follow:

1. connect the sensortile to PC via USB and STLink as picture with battery unconnected

FedericaBossi_0-1734685720947.png

 

2. open the STCubeProgrammer and set STLink as programmer

3. connect to the sensortile, now can you see the flash memory content

click the second icon, browse the BLEFOTA_BL_1.0.0.bin file in the FOTA folder (https://www.st.com/en/embedded-software/stsw-mksbox1-bl.html) and set all parameters as in the picture below:

FedericaBossi_1-1734685720973.png

 

4. start program

5. then, restart the sensortile (unplug and plug the sensortile USB) and you can see by the smartphone app the board ST.BOOT

6. connect to st.boot and you see the firmware upgrade request

7. start the firmware upgrade, when the upgrade is terminated, restart the sensortile and the smartphone app

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.