Skip to main content
SAbba.1
Associate III
August 4, 2023
Question

SensorTile

At the moment I am making an application for 3D sound detection, in which I am making use of the STEVAL-STWINKT1B and the STEVAL-STWINMAV1 microphone array (which I haven't used yet). I am just starting, and I can not understand the operation of the SensorTile, previously I was using the SensorTile.box and it was easier to handle APP ST BLE SENSOR, in which I could easily extract the data, however, in the SensorTile it is getting complicated, I guess it is because of the FW used that I can not see the APP as in "cap2" and rather I see it as in "cap1".

Finally, speaking of the microphone array, I would like to ask how to connect it to the device? physically I have already connected it (in the CN4) but I understand that this is not enough to make use of it (besides I am not very clear how to receive the data that it gives me).

Sorry for so many doubts.

This topic has been closed for replies.

7 replies

niccolò
ST Employee
August 4, 2023

Hi @SAbba.1 ,

it seems that on the board you have the FP-SNS-DATALOG1 firmware, that is able to record data on the sdcard of the STWIN. 
Try to program it with the X-CUBE-MEMSMIC1 firmware instead, so that you can be able to look into the data you need =)
you can find all the info in the examples and in the documentation inside that packet

If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community

Niccolò

 

 

 

 

SAbba.1
SAbba.1Author
Associate III
August 16, 2023

From what he told me I used the "AMicArray_Microphones_Streaming" folder located under the applications folder "STM32CubeExpansion_MEMSMIC1_V5.7.0" that he recommended me to use, for which through the STProgrammer I flashed the FW "AMicArray_4ch_96KHz" located in "STM32CubeExpansion_MEMSMIC1_V5.7. 0\Projects\STM32L4R9ZI-STWIN\Demonstration\AMicArray_Microphones_Streaming\Binary", then I have connected STWIN with STLINK-V3MINI both to the PC, and I have managed to open the file "AMicArray_Microphones_Streaming" in the STCube, my problem now is that I have to run the example to see its working, but my problem is that I don't know how to do this, sorry for the inconvenience, thank you very much.

niccolò
ST Employee
August 16, 2023

Hi @SAbba.1 ,

first of all, if you managed to flash the binary on the board, it is not needed to also run the program in the STCube
you can see on the readme file in the project folder, that
"The board is recognized as a 4 channels USB microphone, allowing the user to easily record the
signals on a host device using any recording software."
so, you should just have to check if the board is recognized as a microphone and then use your software of choice to record it.

then, if you want to change something in the code itself, and check it out rapidly in debug mode, you should use the "run and debug" icon (or something like that, you can recognize it because the icon resembles a bug)
you can find different tutorials on this ST youtube web page =)

hope this helps

Niccolò

niccolò
ST Employee
August 21, 2023

Hi @SAbba.1 ,

so now you are managing to record audio, the problem is that it's not from the mic array, right?

in this case, can you confirm that the connections are right?
(maybe post a photo of the setup)

Niccolò

SAbba.1
SAbba.1Author
Associate III
September 10, 2023

Captura de pantalla 2023-09-10 123827.jpgWhatsApp Image 2023-09-10 at 12.34.30.jpeg

I don't know if there is anything else to do, but from what I read in the manual it was just to connect the microphone array to the CN4 of the board (SensorTile).

I follow the indications in this pdf but I get this error when recording:

audacity.jpg

error.jpg