Skip to main content
Khaled Aljehani
Associate III
September 23, 2017
Solved

Sensitivity of LIS3MDL (LSB/Gauss)

Posted on September 23, 2017 at 05:45

I am using LIS3MDL sensor and I do not understand the sensitivity which its unit is LSB/Gauss.  

In x-cube-mems1 library, the following is calculated:

&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_4G    0.14 /**< Sensitivity value for 4 gauss full scale [mgauss/LSB] */

&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_8G    0.29 /**< Sensitivity value for 8 gauss full scale [mgauss/LSB] */

&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_12G    0.43 /**< Sensitivity value for 12 gauss full scale [mgauss/LSB] */

&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_16G    0.58 /**< Sensitivity value for 16 gauss full scale [mgauss/LSB] */

and in the datasheet:

0690X00000603jKQAQ.jpg

My question is how did they calculate the sensitivity in the above code? and also what does LSB/Gauss mean?

Thanks in advance. 

#lsb/gauss #lis3mdl
    This topic has been closed for replies.
    Best answer
    September 23, 2017
    Posted on September 23, 2017 at 09:33

    Regarding the values in the code mentioned in the cube library:

    For +/- 4 gauss, the sensitivity is 6 842 LSB / gauss, meaning 6 842 = 1 gauss, 12 964 = 2 gauss, 19 806 = 3 gauss, etc...

    However, one way to interpret the data is to read the raw value and display as miligauss.

    If 1 gauss = 6 842, then 1 000 mgauss = 6 842, meaning 1 000 mgauss / 6 842 = 0,146156 mgauss / LSB.

    The same applies to the other ranges. It is just a different look at the same data.

    I personally prefer to keep the precision and use integer math as much as possible in microcontrollers, which is why I wrote my own 'driver' to read, compute and display the values from the sensor.

    6 replies

    September 23, 2017
    Posted on September 23, 2017 at 09:25

    Hello,

    have a look at this earlier discussion, I had the same question before:

    https://community.st.com/0D50X00009XkXwiSAF

    David

    Best answer
    September 23, 2017
    Posted on September 23, 2017 at 09:33

    Regarding the values in the code mentioned in the cube library:

    For +/- 4 gauss, the sensitivity is 6 842 LSB / gauss, meaning 6 842 = 1 gauss, 12 964 = 2 gauss, 19 806 = 3 gauss, etc...

    However, one way to interpret the data is to read the raw value and display as miligauss.

    If 1 gauss = 6 842, then 1 000 mgauss = 6 842, meaning 1 000 mgauss / 6 842 = 0,146156 mgauss / LSB.

    The same applies to the other ranges. It is just a different look at the same data.

    I personally prefer to keep the precision and use integer math as much as possible in microcontrollers, which is why I wrote my own 'driver' to read, compute and display the values from the sensor.
    Khaled Aljehani
    Associate III
    September 24, 2017
    Posted on September 24, 2017 at 06:32

    Thanks

    Koudela.David

    ‌ for your reply. It helped me alot.

    I still did not get it 100%.

    The original equation is:

    magnetic_intensity (in gauss) = raw_data / sensitivity

    So, for this equation the sensitivity is a value from the table in the datasheet(6842 or 2..etc)

    Am I correct here?

    Now, regarding LSB/gauss. What I understand is

    6842 LSB = 1 gauss,

    6842 LSB = 1000 mgauss

    So, sensitivity = 6842/1000 = 6.8

    My question is why did you calculate it in that way? (1000 mgauss / 6842 LSB = 0.14)

    Last thing, in the cube library, they use this equation: mgauss = raw data * sensitivity.

    Should not we use this one (magnetic_intensity (in gauss) = raw_data / sensitivity)?

    Again, I really appreciate your help.

    September 24, 2017
    Posted on September 24, 2017 at 17:56

    Hello

    khaledaljehani99

    ‌,

    Khaled Aljehani wrote:

    The original equation is:

    magnetic_intensity (in gauss) = raw_data / sensitivity

    So, for this equation the sensitivity is a value from the table in the datasheet(6842 or 2..etc)

    Am I correct here?

    Yes, you are.

    Now, regarding LSB/gauss. What I understand is

    6842 LSB = 1 gauss,

    6842 LSB = 1000 mgauss

    So, sensitivity = 6842/1000 = 6.8

    My question is why did you calculate it in that way? (1000 mgauss / 6842 LSB = 0.14)

    Last thing, in the cube library, they use this equation: mgauss = raw data * sensitivity.

    Should not we use this one (magnetic_intensity (in gauss) = raw_data / sensitivity)?

    There are at least two ways of calculating the output value, if you know that the sensitivity is 6 842 LSB per 1 gauss (=1 000 mgauss) and the sensor gives you output of

    –32,768 to 32,7

    1)

    magnetic_intensity = raw_data / sensitivity

    with the following units:

    [gauss] = [LSB] / [LSB/gauss]

    so sensitivity is represented here as[LSB/gauss]

    This relates to the values printed in the datasheet and discussed in the linked discussion.

    2)

    magnetic_intensity = raw_data * sensitivity

    with the following units:

    [gauss] = [LSB] * [gauss/LSB]

    so sensitivity is represented here as

    [gauss/LSB] (which is an inverted value)

    The fact whether you count with gauss or miligauss doesn't affect the equation, just the sensitivity coefficients (and/or the result).

    This relates to the values in the Cube library.

    0.14 < Sensitivity value for 4 gauss full scale [mgauss/LSB] (= 0,000 14 gauss/ LSB)

    0.29 < Sensitivity value for 8 gauss full scale [mgauss/LSB] (= 0,000 29 gauss / LSB)

    0.43 < Sensitivity value for 12 gauss full scale [mgauss/LSB] (= 0,000 43 gauss / LSB)

    0.58 < Sensitivity value for 16 gauss full scale [mgauss/LSB]

    (= 0,000 58 gauss / LSB)

    -----

    ST chose version 2, however, I like version 1 more. Version 1 can be faster and use less resources, moreover, with a higher precision!

    If the sensitivity was a round number in both cases, it would perform the same, but it is not in this case.

    Example 1:

    If the sensor gives you an output of 6 842, method 1 will tell you that the output is 1 gauss. Method 2 will tell you that the output is 957 mgauss (about 4 % difference). (This also comes from the fact that

    0,146156 mgauss / LSB was rounded to 0,14, not 0,15 as I would expect).

    You might say that method 1 output only an integer value in gauss and that you want output in miligauss. There is no problem with that, just multiply the raw_data with a 1000 and you get a 1000 x bigger result (which is what you need, because 1 gauss = 1000 mgauss).

    Example 2, raw data = 10 000:

    Method 1:

    magnetic_intensity [mgauss] = ( raw_data * 1 000) / sensitivity

    magnetic intensity [mgauss] = 10 000 000 / 6 842 = 1 461 mgauss (=1,461 gauss)

    Method 2:

    magnetic_intensity [mgauss] = raw_data * sensitivity

    magnetic_intensity [mgauss] = 10 000 * 0,14 = 1 400 mgauss ( = 1,400 gauss) =again, about 4 % error

    However, method 1 has a downside - if you multiply an output value (by a 1 000 in this example), make sure your data type will handle this.

    In this case sensor raw_data is –32,768 to 32,767 , multiplied by 1 000 gives us -32 768 000 to 32 767 000 and this easily fits into a signed int32 with –2,147,483,648 to 2,147,483,647 range.

    You can the code of method 1 on your own, just call the method below with raw_data as signed int16 as a parameter.

    #define DECIMAL_3DIGIT_FACTOR 1000u // 3decimal points multiplication

    #define COUNT_TO_GAUSS_4G_SCALE 6842; // measured data count per 1 Gauss, full scale +/- 4 g

    #define COUNT_TO_GAUSS_8G_SCALE 3421; // measured data count per 1 Gauss, full scale +/- 8 g

    #define COUNT_TO_GAUSS_12G_SCALE 2281; // measured data count per 1 Gauss, full scale +/- 12 g

    #define COUNT_TO_GAUSS_16G_SCALE 1711; // measured data count per 1 Gauss, full scale +/- 16 g

    // converts magnetometer data (hex) to Gauss unit

    int32_t MM_Convert_To_Gauss (int16_t magnetometerData) {

    int32_t mgaussData;

    mgaussData = (magnetometerData * DECIMAL_3DIGIT_FACTOR);

    mgaussData /= COUNT_TO_GAUSS_4G_SCALE;

    return gaussData;

    }