Skip to main content
Associate III
September 20, 2024
Question

Sensitivity of LIS2DW12 Accelerometer

  • September 20, 2024
  • 1 reply
  • 649 views

Greetings

I am working with the LIS2DW12 accelerometer. I am using the device in Low Power Mode 1, with a FS = +-4g.

According the application note AN5038, page 15, it says that the Low power mode 1, entails a 12 bit value. Thus, using the 16-bit value from the output registers for each axis, it should be divided by 4, and multiplied by 1.952:

 

 

Acceleration in mg = (16 bit hex value from both output registers)/4 * 1.952
Acceleration in mg = (16 bit hex value from both output registers) * 0.488

 

 

 

However in the GITHUB example code, found at the link (line 128)

 

 

float_t lis2dw12_from_fs4_lp1_to_mg(int16_t lsb)
{
 return ((float_t)lsb) * 0.122f;
}

 

 

 The above code snippet shows that the 16-bit hex value from both output registers, should be multiplied by 0.122. 

I am not sure how to make sense of this. 

Any help would be appreciated.

 

 

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
November 8, 2024

Hi @ZAIDS-S23 ,

 

The github example is in high performance mode and thus at FS=4g it is: 0.488/4, in LPM1 the right formula is yours.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.