Skip to main content
MAndr.233
Associate II
August 4, 2020
Question

Sending large amount of data with USB

I'm currently facing a big problem. I've an MCU (STM32L4) connected to an SD card (SDIO) which stores tons of data (5Gb) from a microphone (ST MEMS). I need to send this data as fast as possible from SD card to my PC. With a serial port this is to slow, since the max baud rate of my MCU is 115kb/s.

How can I solve this? I'm thinking about using an FTDI module but for what I'm reading the speed is always limited by MCU baud rate. Best Regards

This topic has been closed for replies.

11 replies

waclawek.jan
Super User
August 4, 2020

Hardly is there a faster transfer method than to pull the SD card from the STM32 board, and push it into the PC (maybe through a USB-connected reader).

You can use UART with a UART-USB bridge at few-MHz rate, with s bit of care. There are also parallel-connected FTDI devices, possibly to be connected through FMC (although I'm not sure about the details).

JW

Pavel A.
August 4, 2020

Eject the card, insert it into PC. Insert new empty card into STM32.

-- pa

MAndr.233
MAndr.233Author
Associate II
August 4, 2020

I cant. It must be with usb cable. I just need anything like 5MB/s

Pavel A.
August 4, 2020

If your USB is full speed... good luck. Try to reduce the data before sending out.

waclawek.jan
Super User
August 4, 2020

There are SD card readers with USB cable. Multiplex the SD card pins between STM32 and the reader.

JW

MAndr.233
MAndr.233Author
Associate II
August 5, 2020

Hum... I'm seeing what your are talking https://www.amazon.com/Anker-Portable-Reader-RS-MMC-Micro/dp/B006T9B6R2. Do you have any idea how this modules works to ensure such high speeds?

Best Regards

waclawek.jan
Super User
August 5, 2020

> Do you have any idea how this modules works to ensure such high speeds?

It's a custom chip implementing USB3 SuperSpeed protocol (plus of course the whole USB stack including MSC, plus the SD "master").

JW

TDK
August 5, 2020

You can get around 100 Mbps with high speed USB. Won't get more than around 6-8 Mbps with full speed.

Implement USB directly on the chip if you want fast speed. Transferring it over UART to an FTDI chip will be even slower.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MAndr.233
MAndr.233Author
Associate II
August 5, 2020

Do you have any idea if it will be hard to implement USB on chip. Has ST anything to help me on that. Furthermore, has ST any drivers to install on PC to support USB protocol?

TDK
August 6, 2020

There are example programs in the CubeMX repository. Here are a few of them:

https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/32L496GDISCOVERY/Applications/USB_Device

JW makes a good points below about USB speed limitations.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
August 6, 2020

You did not tell us exactly which STM32 you use, but generally, on 'L4, there's only Full Speed USB.

JW