Skip to main content
Associate
January 14, 2024
Question

Self test in IIS3DWB

What is self-test in IIS3DWB and what is the criteria to indicate pass or fail??

This topic has been closed for replies.

3 replies

Federica Bossi
ST Technical Moderator
January 16, 2024

Hi @Aalekh ,

Welcome to ST Community!

The embedded self-test functions allow checking the device functionality without moving it. When the self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. 

The completed procedure is described in the section 8 of AN5444:

FedericaBossi_0-1705419600036.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
AalekhAuthor
Associate
January 22, 2024

What to do if Self-test data is not in specified range?

Federica Bossi
ST Technical Moderator
January 22, 2024

Hi @Aalekh ,

It means that the self test failed.

Can you share the output values with and without self-test enabled? Which FS did you set? Please note that the values we give are for 2g. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.