Skip to main content
mats239955_stm1
Visitor II
February 17, 2016
Question

Self test fail

Posted on February 17, 2016 at 14:36

We have a LIS3DH accelerometer that have ended up in a latch-up state. The output data is -205/-1149/-4759 (X/Y/Z in mg). When performing the self test, the absolute difference between the 2 samples are 7/6/3 (X/Y/Z in mg) which is well below the min limit (> 60mg). Is there any way to recover from this? Do I have to make the accelerometer powerless?

#latch-up
This topic has been closed for replies.

1 reply

ferrarofcf
Associate III
February 17, 2016
Posted on February 17, 2016 at 15:15

I use LSM303D and sometime falling in an state of maximum data out on all axis.

Power down, reset ecc. not wake the accelerometer.

The one solution is a strong shock/crash several times and the accelerometer starts running again.

This is really a problem ... and we do not know how to solve it.

It seems a problem similar to yours.