Skip to main content
digidhamu
Associate III
May 9, 2022
Question

Run HS Datalog from Raspberry Pi 3B to Collect Data from STEVAL-STWINKT1B

  • May 9, 2022
  • 1 reply
  • 824 views

As per the Release Notes (v2.4.0 / 5-Nov-2021) for HS DataLog CLI example, I could see executable and libs are present under directory Utilities/cli_example for Raspberry Pi 3B. I have also exported and set the shared library path using command.

export LD_LIBRARY_PATH=<Utilities/cli_example/bin>

But when I execute below command

./bin/cli_example_rpi3b -f ../STWIN_config_examples/DeviceConfig.json -t 100

I am getting following error error.

./cli_example_rpi3b: error while loading shared libraries: libhs_datalog.so: wrong ELF class: ELFCLASS64

Could you please advise whether I am doing anything wrong?

    This topic has been closed for replies.

    1 reply

    SimonePradolini
    ST Technical Moderator
    July 22, 2022

    Hi @digidhamu​,

    To overcome any kind of configuration issues, we will provide a configuration script for linux and raspberry in the FP-SNS-DATALOG1 v1.4.0.

    This new version will be available by the end of July/first days of August.

    You will just lunch the raspberry_setup/setup_rpi3b.sh script, and then everything should work properly.

    I suggest you to update the CLI once available.

    In your use case, you are loading the entire /bin folder, that contains both Linux and Raspberry .so version.

    The Linux one (libhs_datalog.so) can't work on Raspberry and maybe that's the reason for the error.

    Move libhs_datalog.so into another folder and launch newly the script.

    Do you still have the same error?

    Best regards

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.