Skip to main content
Visitor
Jul 23, 2026 11:15 PM UTC
Solved

Regarding the temperature characteristics of the IIS2ICLX

Regarding the behavior of temperature drift of the IIS2ICLX, I would like to ask for your guidance.

- When the temperature increases, how does the zero-point temperature drift behave?

- Does the amount of zero-point drift change depending on the rate of temperature increase?

For example, after heating rapidly to 80°C and then allowing the temperature to stabilize sufficiently, compared with slowly heating to 80°C and allowing the temperature to stabilize sufficiently.

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 29, 2026 1:52 PM UTC

Hi ​@Tomohiro ,

The zero-point temperature drift of the IIS2ICLX is primarily determined by the final stabilized temperature. A faster temperature ramp can introduce additional transient offset due to thermal gradients and mechanical stress, but once the sensor has fully stabilized at 80∘C80​∘​​C, the steady-state zero-point should be essentially independent of the ramp rate.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

Federica Bossi
Federica BossiBest answer
ST Technical Moderator
Jul 29, 2026 1:52 PM UTC

Hi ​@Tomohiro ,

The zero-point temperature drift of the IIS2ICLX is primarily determined by the final stabilized temperature. A faster temperature ramp can introduce additional transient offset due to thermal gradients and mechanical stress, but once the sensor has fully stabilized at 80∘C80​∘​​C, the steady-state zero-point should be essentially independent of the ramp rate.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.