Skip to main content
NKuhn.1
Associate
August 31, 2022
Question

Read lsm6dso32 data via libiio

We are trying to use lsm6dso32 accelerometer/gyroscope connected to a custom hardware (non-st) via i2c. What we want to achieve is reading measured values continuously, ideally via libiio (buffered).

We are building a custom linux (kernel version 5.4) via yocto for our board and integrated this driver for lsm6dso32 support into it: github.com/torvalds/linux/tree/master/drivers/iio/imu/st_lsm6dsx.

Question 1:

Is the driver integrated in the kernel sources the same one, ST is providing here?

github.com/STMicroelectronics/STMems_Standard_C_drivers

Question 2:

If we are using the driver st_lsm6dsx from kernel sources, do we still have to apply the changes stated out here?

github.com/STMicroelectronics/STMems_Linux_IIO_drivers

So would we have to patch include/uapi/linux/iio/types.h to add custom events, for example, to be able to read data?

Question3:

Ideally, we would like to use libiio to read lsm6dso32 data. We are currently failing to do so because enabling iio devices for gyro and accelerometer is not possible and creating a buffer fails (respective libiio docs: analogdevicesinc.github.io/libiio/v0.19/index.html). We do see sysfs nodes/folders for accelerometer and gyro in /sys/bus/iio/devices/, but within their device folders, there are no scan_elements or buffer folders. Is it even possible to use libiio to read lsm6dso32 data? Did anybody else tried the same and could provide some informations/example code/configuration? Or do we have to use and adapt c code provided here instead of libiio?

github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm6dso32_STdC/examples

Any help would be very much appreciated.

(sorry, had to remove protocol prefix from all my links, because seems like, I am not allowed to add links to my post/question...)

    This topic has been closed for replies.

    3 replies

    NKuhn.1
    NKuhn.1Author
    Associate
    September 1, 2022

    Added this issue in github to increase attention: github.com/STMicroelectronics/STMems_Linux_IIO_drivers/issues/15

    Eleon BORLINI
    ST Employee
    September 1, 2022

    Hi @NKuhn.1​ ,

    right, I believe that the best solution is to open an issue directly on Github.

    Let me know if you get an answer there

    -Eleon

    NKuhn.1
    NKuhn.1Author
    Associate
    September 1, 2022

    Just for clarification: The issue I opened is located in ST's github repo of the driver, not the official linux kernel driver.