Skip to main content
Pasi MYLLYMAKI
ST Employee
May 11, 2020
Question

Question from Predictive Maintenance Webinar 29th of April: The ODR of the data logs changes from the set ODR, in fact we have measured ODR which can be more than 5 % different from the set ODR. why is so...

..

    This topic has been closed for replies.

    1 reply

    Vladimir JANOUSEK_34072
    Visitor II
    May 12, 2020

    There are naturally some tolerances in the internal clock source in each particular sensor and this is the reason why also ODR has some tolerance. It is possible to monitor the exact ODR on the fly by means of DRDY interrupt from the sensor and e.g. and accurate timer in the MCU. ODR tolerance level depends also on the exact sensor component model.